AnsweredAssumed Answered

Can I get updated firmware for 34970A? What changes exist?

Question asked by drkirkby on Jun 9, 2019
Latest reply on Jun 10, 2019 by Tardz

I have an old HP 34970A, which identifies itself on the bus as

 

HEWLETT-PACKARD,34970A,0,8-1-2

 

If my understanding is correct, that means

 

8 is the firmware revision for the measurement processor

1 is the firmware revision for the input/output processor

2 is the firmware revision for the front panel display processor.

 

Can the firmware be updated, and if so how? Is there a change log, so one can see if there are significant changes, or just very minor ones?

 

Dave

Outcomes