I am looking for a Windows XP SP3 Restore Image for the 16902a Logic Analysis System. It seems nowhere to be found on the main web-site. The goal is to instal the Logic and Protocol Analyzer Software v5.90, but it requires WinXP SP3, and won't install on WinXP SP2 that is currently installed on the device.
We have no restore images with SP3. The only thing you can do is use an XP restore image, get the system running as a PC, then install an SP3 update downloaded from the web. There are multiple sites where they are available.
Note that there are different 16902B restore images, depending on the Serial Number of the unit. If you post the SN, I'll reply with a link to the correct restore image in DropBox. I may also have an SP3 image there. I haven't looked recently. For a while, DropBox was deleting images like that, due to potential copyright issues.
Al