AnsweredAssumed Answered

E4418B READ? returns only single digit numbers.

Question asked by tbayler on Jun 7, 2019
Latest reply on Jun 10, 2019 by Tardz

I am reading -14.44dBm on the display and when I execute a READ? or MEAS? or FETCH? it will return my number as -1.444...If I'm reading -9.85dBm on the screen, the READ? etc..returns a solid measurement in the correct format.  I have read through the programming manual and cannot find why it would not return my numbers as it is displayed on the screen.  Any help is much appreciated!  

 

thanks!

Outcomes