I'm new to the Genesys software, and I want to make sure I'm not skipping anything. If I wanted to add a Coilcraft Wideband Bias Choke would I just drop in a generic inductor using the 'L' hotkey and adjust the parameters by double clicking on it? Is it important/possible to add the S-Parameter files provided by Coilcraft to the part model? I didn't see anything quite like this in the tutorial videos that came with the software.
To import s-parameter files, do the following steps:
File > Import > Circuit Files > S-Data File...
Choose your file.
You then will see a node in the project tree with the new .snp file. You then drag that over to the schematic and connect it for your needs. I don't think you can create a .snp model from a device like C, L, R, etc. I also don't know of a way to edit a model to do that. There may be but I don't know of it. I do know that importing it works ok.