I wish to save the state of an 8753 to a floppy drive, with a name of my choosing - not FILE00, FILE01, using GPIB, but can't seem to work out what commands to use.
I can do this from the front panel by saving the state, which gets saved to a FILE00, FILE01 etc, then rename the file, but it is a lot of messing around.
INTD - selects internal floppy disk
STOR<n> - saves states 1 to 5
but I can't work out how to save a file with a particular name. If for example I wanted to save the state, under the name FOOBAR, how can it be done?