AnsweredAssumed Answered

Synchronizing VNA with Signal Generator

Question asked by Eshar on Aug 23, 2010
Latest reply on Aug 24, 2010 by gfarrel
I want to synchronize the sweep of my PNA (E8361A) and my Signal Generator (E8257D) so when the PNA is sweeping from, let's say, 1 GHz to 60 GHz the Signal Generator will follow.

From my understanding, I will need to connect the 10 MHz references of the two tools together and possibly use the Sweep In/Out. However, I haven't done this before and I like to get some concrete instructions on the setup.  

Outcomes