AnsweredAssumed Answered

Problem in inerfacing CEC'S PCI GPIB 488 CARD with e4980A

Question asked by manish on Jul 18, 2007
Latest reply on Jul 19, 2007 by odanzy
I have purchased An Agilent e4980A LCR meter and a CEC PCI GPIB 488 for data transfer purpose. The problem is that The GPIB does not detect the instument. The I/O Library provided with the instrument is not able to detect the instrument via GPIB( rather it works with the LAN and USB modes). The interactive tool shows that the "instrument is not connected ".
However I/O detects the GPIB.  

Outcomes