AnsweredAssumed Answered

Edit traces in Strip Chart, VEE

Question asked by CyberLeffe on Jul 11, 2007
Latest reply on Jul 11, 2007 by Adrian
I just can´t make the Traces in the "Strip Chart" in VEE to work. I want to use the input to change the names of the traces. I have managed to change one name but when I try to change more then one I run in to problems.

I have made a constant record with two fields with the names "TraceNum" and "Name". When the "TraceNum" is a Int32 scalar and the "Name" is an Text scalar it works. But the you are only changing one name. And I want t change more then one using a single record.

Image

Outcomes