AnsweredAssumed Answered

SQiDD board vertical probe contacts

Question asked by gprice on Apr 15, 2019
Latest reply on Apr 15, 2019 by gprice

Has anyone had a need to replace the vertical scope probe contacts on the SQiDD board?  Mine are wearing out and need to know if there is data about the manufacturer of these contacts and their internal part number.  For reference these are located at testpoints 3, 4, 7, 8, 11 and 12 on the E2646 board.  It is a low/full speed SQiDD.

Outcomes