AnsweredAssumed Answered

8753B Opt 006

Question asked by djn@ieee.org on Nov 27, 2011
Latest reply on Nov 29, 2011 by RayH
Hi all...First post...

The 8753B I have signs on with a screen noting installed options = 006. However, I cannot find anything under the System menu for this.

I have been informed that unless I attach an 8587A test set with doubler that the menu will remain hidden. As I don't have the test set, I need to confirm if option 006 is in fact installed.

Any hints on this?

Dan in Chandler, AZ  

Outcomes