AnsweredAssumed Answered

Hello , I'm using current probe to measure dc current with frequency of 5.6MHz , but I don't get the current pulse at the said frequency but at 1khz. Should i get the current at 5.6Mhz or what else can be the reason ? The probes bandwidth is of 50MHz and

Question asked by chipmate008 on Apr 4, 2019

Hello , I'm using current probe to measure dc current with frequency of 5.6MHz , but I don't get the current measurement at the said frequency but at 1KHz. Should I even get the current at 5.6Mhz or what else can be the reason ? What if the current readings shown by probe are average current rathar than peak current.

 

Probe spec : 30A , 50MHz AC/DC

Outcomes