Hi,
Would it be possible to sweep a frequency range and alter the Vpkpk sinewave from the signal generator depending on either the reading from the digital mutlimeter achieving a known value or a maximum level on the Signal Generator which ever one is comes first?
Typical values:
Frequency Digital mulitmeter Or Max Signal vpkpk | Amplitude V | RMS mV |
100 | 3 | 600 |
200 | 3 | 600 |
400 | 3 | 600 |
500 | 3 | 600 |
600 | 3 | 600 |
700 | 3 | 600 |
is this sesquence possible utilising test flow?
Many Thanks