AnsweredAssumed Answered

IVI DCPwr Driver Generates Invalid Value Error

Question asked by hwu on Mar 28, 2019

I'm working with N6705C with the IVI driver and getting an invalid value error when I try to set the trigger source. The attached is the NI I/O trace that captures the SetAttribute command. It works with the attribute value 0 and 2 only. All other values generate the same invalid value error. Any idea why?

Outcomes