AnsweredAssumed Answered

Scalar Network Analyzer(SNA) Agilent 8757D Control

Question asked by Natty on Apr 21, 2008
Latest reply on Apr 22, 2008 by RayH
I am replacing an old SNA with Agilent 8757D instrument.  I can only get it to work if I use it as Address 16 through GPIB.  When I change the address to the desired address (5), the 8757D will try to passthrough commands to all bus instruements.  I have turned SYSINTF to OFF, and the Sys Bus is NOT connected.  this device interferes with all the instruments on the bus unless i revert it to the default address (16)

Is there a way to disable the passthrough and change GPIB address, where it works?

-Natty  

Outcomes