AnsweredAssumed Answered

Sequence does not trigger on External Trigger but works on Manual Trigger

Question asked by hramanna on Mar 13, 2019
Latest reply on Nov 4, 2019 by Tardz

I created a sequence on the Waveform Builder Pro application. The sequence basically repeats 0V until a trigger, produces a ramp to 0.8V and then stays at 0.8V indefinitely.

 

After I transfer the sequence onto the Function Generator (33511B), I set the trigger to be external and hook up a pulse generator to the back-panel (0 to 3V). This does not trigger the ramp.

 

If I change the trigger to be manual, the sequence works correctly. 

 

How would I change the sequence to take an external trigger?

Outcomes