Hallo,
While using si pi pro in ads 2019, i get an error
exception caught in fem_process: source < c6> is isolated from the problem domain.
Make sure that the source is not defined along a PEC object and it is not within an unmeshed metal.
c6 is a capacitor which is connected between the board ground and ground.
However, in ads2017, this error doesnt arises . Is it because of any settings change. If so, how can I rectify it?
Kindly reply.