AnsweredAssumed Answered

Loading dual channel waveforms from USB on 33522A.

Question asked by TechEngineer on Feb 16, 2019
Latest reply on Feb 16, 2019 by Tardz

Hi, I have a dual channel waveform that I created on benchlink waveform builder. I can load that dual waveform to the generator through direct USB connection to the PC or Ethernet, and all is well. But if I save the waveform on a USB stick and try to load the waveform through the USB front panel, I get an error that "Dual channel waveforms are not supported".

 

Why is this happening? This is really important on the field as it's not always practical to carry and use a laptop at the same time.

Outcomes