AnsweredAssumed Answered

Creating pulse waveform using VEE for Keithley volt device

Question asked by neilhutcheon on Mar 23, 2007
Latest reply on Mar 23, 2007 by odanzy
I'm having trouble in creating a suitable program on VEE which will allow me to produce a pulse waveform, at no higher than 20Hz, pulsing from 0-50V.

I'm writing to a Keithley programmable voltage source model 230, and the pulse generator function provided on VEE is not recognised by the device.

I have also tried to create my own loop, setting an initial voltage of 0V then setting a delay and a final command for 50V. This is working although I cannot find a way to allow this to run continuously until a break command if called. Is there a way in which this could be achieved?

I assume this must be a fairly straight forward task but my lack of knowledge in VEE is providing some difficulty.

Thanks for your help.  

Outcomes