Hello,
I am using N5242A with A.09.90 firmware. I would like to perform current measurements in pulsed mode using N2782B current probe with 34465A multimeter. I am trying to add external DC Meter according to: Configure a DC Device.
In the "Enable I/O" box I set the following commands:
conf:volt:dc;
trig:count 201 (number of points);
trig:sour ext;
trig:slop pos;
trig:del 0;
samp:count 1;
Which means, DMM uses external triggering, and captures 1 sample per trigger.
In the "Before Sweep" box: I set the following comand:
INIT
in the "After sweep" box:
FETCH?
However, the DMM returns errors. How to perform this measurement?
Best regards,
Pawel
Hi, I tested your sequence on my 34410A with success. The 34465A is the replacement of 34410A. I tried with slow or very fast frequency trig without problem. Input trigger source must have between 3 to 5 V and pulse width min is 1µs.
hoping that this information can help you.
Yves