My PNA 5321A has had an error splashed across the display for a few months - "Unleveled source 1, out 1". I've finally gotten around to "clearing" the error, using the helpful info on this forum. I found these two to be quite useful:
https://community.keysight.com/thread/4245
https://community.keysight.com/message/69834
I tried changing my power levels, my frequency ranges, pushing the "Preset" button, then finally running the operators check. The operators check reported several errors. I'm a software guy, not expert with Network Analyzers. Just wanted to ask you guys how likely it is that I'll need to send the unit in for repairs. Is it possible that I've configured the PNA somehow to cause it to fail these tests? Is there anything else I should try? Attached is the configuration of my unit, and the results of the operators check. Thanks.
Something is seriously wrong with this unit. Assuming you have all the front panel jumpers (if any) in their default position, then the PNA should pass the OpCheck. The errors shown indicate the source (or the synth feeding the source) is bad. I would send it in for repair.