I am designing a passive feed network for an Antenna array. The network consists of many couplers and symmetrical/asymmetrical splitters, filters and more. I simulate each of the elements separately in a schematic sheet, but at the end I want to combine and make a full layout of the network, and connect them together.
My problem is when I make a sub-circuit from a schematic, I do not know how to insert in my high level schematic that it also Include the layout.
If I drag and drop it uses a 3/4 port network as a data set and a default footprint instead of the actual layout.