AnsweredAssumed Answered

Saving Spectrogram of specific length N9020B

Question asked by Yan.Fett on Jan 11, 2019
Latest reply on Jan 16, 2019 by Yan.Fett

Hello,

i currently send the following commands:

'INITiate:CONTinuous 0' # Set Measurement mode to single instead of continuous

XXX # Do 200 Measurements
'INITiate:IMMediate' #Clear everything that happened before and start the 200 Measurements
'*WAI' # Wait for completition
':MMEMory:STORe:RESults:SPECtrogram "19_01_11_test.csv"' # Store the Spectrogram

 

What i expect it to do, is saving a spectrogram with 200 Traces. I can not find the command to set how many measurements it will do. Also the '*WAI' command does not seem to act as i would expect it to.

Thanks for your help!

Outcomes