AnsweredAssumed Answered

Generating a user correction file using SCPI commands on the E8257D

Question asked by nsm on Jan 3, 2019
Latest reply on Jan 5, 2019 by nsm

Hi, There was a question already on this topic on this in the forum but apparently there was no answer. Re-opening the pandora's box again!! I do understand that we can write a program to control the power meter and signal generator separately to generate the correction table. The programming manual gives an example of loading the frequency, amplitude pairs into the memory. However, I would like to know the following.

  1. How do we initiate a user correction using scpi commands?
  2. if there is a user correction file in the memory, how can we read the frequency and amplitude pairs using scpi commands from the file? 

 

Best Regards

Nsm

Outcomes