AnsweredAssumed Answered

Is it possible to configure the Keysight PNA families of network analyzers to display a time domain transformed trace as impedance versus time or distance (equivalent to the legacy network analyzers 'Z: Refl' mode)?

Question asked by briancamhitachi on Dec 19, 2018
Latest reply on Dec 19, 2018 by tsilchia001

HAVE PNA N5245A XP with options 010 Time Domain capability + options 400 & 460.  QUESTION: NEED TO READ Characteristic Impedance = Z0 of a coax cable 72 ~ spec +/- 3 ohms.  How do I setup to read Z0 @ 2 ns input Impedance ?? Found

Is it possible to configure the Keysight PNA families of network analyzers to display a time domain transformed trace as impedance versus time or distance (equivalent to the legacy network analyzers 'Z: Refl' mode)?  @ Is it possible to configure the Keysight PNA families of network analyzers to display a time domain transformed trace as… 

BUT the Graphic are low res and not clear  --- With the Transform, can measure Time delay, of 10 ft coax -- see attached which matches to our broken 54754 TDR Module, but How to do Z0?? Thank You Brian

Attachments

Outcomes