EMmodel error: Evaluate model for default parameters.
What's wrong with it?
Analysis "Solve" (M181223002726) of design HWRes_lib:R_Concept:layout_defPara_v1 failed:
--- ERROR ---------------------------------------------------------------------
A calibrated pin must not be positioned on an
edge on which other pins are positioned.
(Using a single calibrated pin simultaneously in
several ports is also invalid in this respect.)
The pins involved are "tlineP111_P2" and
"TFR_TaN10_P2".
-------------------------------------------------------------------------------
Consult the Job Manager log for full details.
Log say:
--- WARNING -------------------------------------------------------------------
... Several similar warnings...
The port setup needed to be corrected:
TML calibration for port "tlineP99_P1" has been
changed to TML (zero length) calibration because
the transmission line of pin "tlineP99_P1" would
otherwise intersect with the layout.
-------------------------------------------------------------------------------
Generating mesh at 68 GHz...
--- ERROR ---------------------------------------------------------------------
A calibrated pin must not be positioned on an
edge on which other pins are positioned.
(Using a single calibrated pin simultaneously in
several ports is also invalid in this respect.)
The pins involved are "tlineP111_P2" and
"TFR_TaN10_P2".
-------------------------------------------------------------------------------
Hello,
the error is what the message says: "A calibrated pin must not be positioned on an edge on which other pins are positioned."
It seems that you have two pins (ports) on the same polygon edge. Note that a pin on the edge will result in a port that spans across the entire width of that edge, and doesn't stop at vertices in between. Example: If you have a T-junction and a stub, that might result in one wide edge from of T-junction plus stub, if the are in line with each other.
Regards,
Volker