AnsweredAssumed Answered

Built-in components for parameterized layout

Question asked by Jade on Dec 21, 2018
Latest reply on Jan 11, 2019 by bafisher

In the help doc, ”Defining Component Parameters”->”Using Existing Components”, the doc say that “You can set up a parameterized layout by using a combination of several built-in components”. In the following graph, “em1”is selected as the built-in components. Where does “em1”comes from and how can I refine em1? Are there details docs about the “built-in components” ?

Outcomes