In the help doc, ”Defining Component Parameters”->”Using Existing Components”, the doc say that “You can set up a parameterized layout by using a combination of several built-in components”. In the following graph, “em1”is selected as the built-in components. Where does “em1”comes from and how can I refine em1? Are there details docs about the “built-in components” ?
There are two methods for assigning parameters to layout (lookalike) components:
* Nominal/Perturbed (for arbitrary geometric layout objects, i.e. primitives)
* Subnetwork (for components)
Please see the documentation for more details, or contact your local Technical Support center.