AnsweredAssumed Answered

N3300A VB.NET programming performance improvement

Question asked by lciott on Oct 31, 2018
Latest reply on Nov 5, 2018 by Tardz

Not sure if this is the correct forum, but there is nothing with the N3300A in it, and it is sort of power supply related.

 

I am controlling a N330A DC electronic load from within a VB.NET application using the SCPI.NET drivers via a serial port connection. I have to control the constant current amplitude at a fast rate.  I have been able to go as fast as 30mS when using a python script, but within VB.NET the fasted I can do this is around 80mS. Is there a faster way to to this?

Outcomes