Our hardware setup is:
The AWG is connected to the PSG generator to create the wideband I and Q inputs. Then the RF output is connected via cable to the scope. The VSA software is installed in the scope. I need to synchronize the transmitted signal and the IQ data seen in the VSA software.
To do that, I connected the EVENT 1 of the AWG to the TRI OUT of the scope. When I set the EXTERNAL in the VSA software, it shows waiting for the trigger. It means it's not getting the signal from the AWG. I have attached the screenshot.
Did I connect it wrong?
Any help will be appreciated.
Thanks