AnsweredAssumed Answered

Digital Serial Analyzer Sampling Oscilloscope DSA8200

Question asked by A.E.D on Oct 4, 2018
Latest reply on Oct 8, 2018 by algoss

I have NI measurement system  consist of two chassis VSA & VSG to generate and acquiring the signals. I have connected Oscilloscope DSA8200 to measure the time domain waveform and to check them with the generated waveform from NI receiver system. I started with generating two tones (as per attached) while the 10 MHZ timing is connected with RFS & RFSG to be synchronised and the trigger is connected as an external trigger. 

 

 

I am just wondering if this Oscilloscope is capable of reading these waveform and it is right as shown in attached thread or something else is needed because I am unable to get the waveform from the scope and the NI receiver to be matched. Thanks in advance.

Attachments

Outcomes