AnsweredAssumed Answered

Communication with an E8363B through LAN by Keysight Connection Expert 2018

Question asked by aaawucy on Oct 3, 2018
Latest reply on Oct 5, 2018 by daras

I tried to communicate with an E8363B through LAN by Keysight Connection Expert 2018. It does not seem to work well.

 

The IP address of the E8363B is 192.168.1.7 and the IP address of my laptop is 192.168.1.17. The mask of both is 255.255.255.0, and the gate 192.168.1.1. I pinged the VNA from the laptop. The connection is fine. However, the Keysight Connection Expert 2018 cannot find the VNA. Do you have any idea of this problem, please?

 

Then, I tried to use Keysight BenchVue Troubleshooting Wizard to solve this problem. It says that Agilent License Service is not installed and there is no internet connection. Actually, my laptop can access the internet. Could you give me a suggestion?

 

To make sure the Keysight Connection Expert 2018 is OK, I tried to communicate with an N5183A through LAN by Keysight Connection Expert 2018. It works well. The Keysight Connection Expert 2018 can find the signal generator.

 

Many thanks and kind regards.

Outcomes