AnsweredAssumed Answered

34465A Maximum Sample Rates

Question asked by ealm on Sep 13, 2018
Latest reply on Sep 14, 2018 by Tardz

On page 3 of the Digital Multimeters 34460A, 34461A, 34465A (6½ digit), 34470A (7½ digit) Data Sheet it indicates that the maximum reading rate for DC voltage, current and resistance for the 34465A without the DIG option is 5,000 rdgs/s but on page 20 indicates that the readings/s is 3,333 using an integration time of 0.02 PLC/300 us. Then on page 21 it indicates a maximum internal trigger rate of 5,000/s. Is the sample rate determined by the type of measurement that is being made, e.g. continuous versus data log modes?

Outcomes