AnsweredAssumed Answered

RCS Measurement

Question asked by sudhir on Aug 28, 2007
Latest reply on Aug 29, 2007 by tsilchia001
I want to measure the reflected power with Network Analyzer for RCS measurement. I have the following setup.

4396B and 87512A.
tx/rx antenna connected to the test port of 87512, which is connected to the network analyzer.

Calibration: I used the tx/rx antenna in its position as the load.

I am using the reading at input port R as transmitted power in dBm and that at the input port A as the reflected power. Is that the right way of measuring the reflected power with the Network Analyzer?  

Outcomes