AnsweredAssumed Answered

E5071C - Intuilink problems

Question asked by obranje on Feb 9, 2012
Latest reply on Feb 10, 2012 by obranje
Hi everybody,

I have an E5071C for two years now, and I need some help in order to connect the Intuilink (Installed in WinXP and Win7 machine) to the instrument in order to obtain the data. Until now i´ve been using the USB port.

I already installed the IO Libraries Suite and ran the Agilent Conection Expert and add the instrument in the LAN interface (this is okay). The problem is that my PC can´t connecto to the E5071C.

Could you please help me?
And also, it´s possible to obtain the data from the web server?

Best regards,
Oscar  

Outcomes