AnsweredAssumed Answered

8594E with Prologix USB to GPIB adapter

Question asked by capngene on Dec 13, 2010
Latest reply on Dec 20, 2010 by capngene
Can someone help me connect my 8594E Spectrum analyzer to my computer using Prologix USB-GPIB adapter. I have successfully connected to an 8510 and received plots using John Miles 7470A Emulator. I have used the Prologix Configurator with the 8594 and it seems to recognize the analyzer but when I request a plot it times out with a communication error :?:  

Outcomes