AnsweredAssumed Answered

external trigger duration signal (pna e8364c)

Question asked by fcolleon on Sep 23, 2009
Latest reply on Sep 23, 2009 by Dr_joel
Hi all. I'm thinking on using the "trigger in" function (pin 19 of AUX IO conector). In the manual it says the trigger signal should be between 1-50 us. The device i would be using for trigger the pna has a signal in the ms range(minimun duration is 1 milisecond). Could i use this signal for trigger in the pna? If i use the bnc conector, it can be used tha 1 ms signal? I'm thinking on level trigger(i can set the duration of the signal be logic low or high for 1 ms). Thanks  .  

Outcomes