AnsweredAssumed Answered

Using VEE to access Intuilink COM objects

Question asked by rickhart on Apr 25, 2008
Latest reply on Apr 25, 2008 by odanzy
Does anyone have an example of using VEE to access Intuilink objects?

I'm trying to use VEE to download the 8753E screen image via Intuilink to a bitmap file that we will then save to our network drive (to save paper).

I need to use VEE because I also want to write to the 8753E screen the part number serial number, etc. before downloading the image(I've got this worked out already) then I'll use VEE to write this bitmap to the network drive.

I'm using the following:

Set IDC = createobject("agtDC8753E.IDataCapture");

and then

IDC.PictureBMP;  

It's giving an error "Cannot convert incompatible activeX automation value- empty object reference  error number: 566

Any idea what's going on?  

Outcomes