AnsweredAssumed Answered

8757D, Interrogate Function

Question asked by WDrago on Aug 19, 2009
Latest reply on Aug 20, 2009 by odanzy
All,

I'm working with an 8757D and all of the functions I've tried so far are working well.

However, When I try to use the interrogate function (OP) to read scale (OPSD;) I do get the correct reading back, but then the next command I send will timeout. After the timeout everything starts working fine until I read the sale again.

Anyone have any suggestion as to why this is happening and how to fix it?

Thanks,
Bill  

Outcomes