AnsweredAssumed Answered

IMeasurement getData returns wrong format

Question asked by cgantz2000 on Aug 27, 2010
Latest reply on Mar 26, 2011 by AndrewIsaverdian
I'm using the following IMeasurement8.getData to return S21 data. This used to work correctly, and still works on other PNA's, but now instead of returning LogMag, it is returning linear. The display is showing LogMag, and 20*log of the data gives the results shown on the display. I'm using firmware version A.09.20.06.  Any idea why this would be happening.      

object objS21 = meas21.getData(NADataStore.naCorrectedData, NADataFormat.naDataFormat_LogMag);  

Outcomes