AnsweredAssumed Answered

Intuilink and Windows 7

Question asked by rbarta on Nov 17, 2009
Latest reply on Sep 27, 2012 by tsilchia001
I've recently be upgraded to window 7 and office 2007.  I have used the intuilink tools in the past to pull data and plots from the VNA and PNA network analysers. It appears neither of these apps are compatible with windows 7 and there are not vista versions available.  I have installed the vista version of intuilink for the 33120 ARB and it appears to function properly. Any suggestions for apps that can used or a work around that is nicer than putting s2p files on a floppy and plotting them in excel  

Outcomes