AnsweredAssumed Answered

8757D Learn String troubles

Question asked by WDrago on Jun 1, 2009
Latest reply on Jun 1, 2009 by jvall
All,

I am using an 8757D with a 83650B sig gen. For this project I need to store about 20 different cals. There aren't enough registers in the 8757D to do the job, so I want to use the learn string. I'm assuming the learn string stores cal info as well as the basics like startF/stopF/power. If I'm wrong then the rest of this is irrelevant.

I can read the 300 byte string without any trouble (although most of the data seems to be 0's). The headaches start when I try to load them back to the analyzer. What's the secret? (I'm using VEE 8.0)

Thanks,
Bill  

Outcomes