AnsweredAssumed Answered

E5071B VBA AND LOOP

Question asked by Ganiu on Jul 13, 2009
Latest reply on Jul 13, 2009 by odanzy
I have successfully taken measurement of samples at 1.25 GHz on E5071B. Is it possible to measure the characteristics of samples over a range of frequencies at the same time e.g 6 modes (1.25 GHz, 2.5 GHz, 3.75 GHz, 5 GHz, 6.25 GHz, and 7.5 GHz)in one single measurement rather than taking measurements of each frequency one after the other as I have been doing? Can this be achieved by modifying the VBA code e.g. by introducing a loop or by another means?

Thanks in advance.  

Outcomes