AnsweredAssumed Answered

Data reading problem at PNA by using C

Question asked by fada on Jan 18, 2010
Latest reply on Jan 19, 2010 by fada
Hi,

I connected to PNA network analyzer via ethernet. I can send all "Write" commands by using C# for example adjusting start frequency, stop frequency etc. but I can't read anything from the PNA. For example I sent "*IDN?" command to PNA but c#  send back a timeout error. Contrary, I also use VEE and it works properly. I wrote my c# codes below. I will be very plesant if someone help me. I wrote some comments near the codes.  

Outcomes