AnsweredAssumed Answered

manual trigger via LAN E8364C

Question asked by fcolleon on Apr 13, 2009
Latest reply on Apr 13, 2009 by odanzy
Hi all. I'm interested on using the trigger option for make "point" measurements(with the pna E8364C). But i would like to use the manual trigger via software(LAN, with labview), not via external hardware(AUX connection). Seeing the programing commands, it seems there's only options for the external hardware, and not via software. It could be done? Programming a manual trigger via software(lan, labview), an not via the external aux conection?
Thanks .

Franco  

Outcomes