AnsweredAssumed Answered

How to fix the error PNA E8362B?

Question asked by Hidayah on Mar 10, 2008
Latest reply on Mar 10, 2008 by odanzy
Hi,

Here I attach my vee file . This one got error " I/O error or timeout occured with GPIB at 7 " Error no : 811. Could someone please check what is the problem with my vee file ? Here is the briefing what I want to do with this VEE. An antenna will be connected to port 1 and another antenna will be connected to port 2. I just want to read the power at 2.45 GHz only for port 2 using VEE. I want to repeat the reading for 10 times. Every readings have delay 2 seconds. The readings is displayed in txt file like below.


Frequency (Hz)   Power (dB)

2450000000        -15.19
2450000000        -15.97
2450000000        -16.95
2450000000        -16.87
2450000000        -17.95
2450000000        -18.09
2450000000        -19.17
2450000000        -20.95
2450000000        -22.87
2450000000        -24.95

I had labeled the PNA-L at the IO Libraries Suite and also at the instrument manager. I labeled it as GPIB7 at address 21. Please help me. Thanks.

Regards,
Dayah  

Outcomes