AnsweredAssumed Answered

What is the correct method to set range in SCPI command

Question asked by kent5244 on Jun 16, 2010
Hi all,

I have a problem in write SCPI command to 34401A. I have write the following SCPI command and its works.

DMM.WriteString "Measure:Res? 1000, 0.01"

I know that 1000 is for the range, and 0.01 is for the resolution.

But now i wish to set range by assigning 1000 as minimum and 2000 as maximum. As for resolution is 0.01 as minimum and 0.1 as maximum.

Need some advise.

Thanks,
Regards  

Outcomes