AnsweredAssumed Answered

SCPI guided ECal initialization failed

Question asked by JackVee on Jan 10, 2007
Latest reply on Jan 10, 2007 by JackVee
Hi all,

I want to perform guided ECal on N5230A NA by sending SCPI commands from VEE PRO. The ECal module is N4691-60003 and port connectors are both APC 3.5 female. The VBScript program modified from PNAHelp, running as a macro in the PNA worked. However, when I sent SCPI command to initialize the calibration, it didn't work. The commands sent through DIO are shown in the attachment (PS: only the initialization command didn't work). The error message was:
   
The SCPI command received has caused error number 192: "Guided cal initialization failed".

By the way, I could not find the SCPI error number 192 in PNAHelp. Does anyone know what causes the problem? Can I perform ECal externally?

Thanks,
Jack  

Attachments

Outcomes