AnsweredAssumed Answered

Possible to use E5062A VBA to automate a specific test?

Question asked by StdLabMan on Sep 6, 2007
Latest reply on Mar 28, 2019 by tsilchia001
Hello all, I am starting from the beginning with this VBA question and sort of just looking for a yes or no to get started.  We use the E5062A at my company, and are setting up an insertion loss trace from 950 MHz to 2150 MHz.  We analyze the entire trace to be sure the insertion loss does not deviate more than 1 dB within a 40 MHz span along any portion of the trace.  If it deviates more than 1 dB, we need to know that 40 MHz p-p dB value, and the start frequency of that deviation.  We currently do this by "eyeballing" and manually moving two markers at a 40 MHz span along the trace.

Is it possible to automate the above using the built in VBA programming?

As mentioned above, just maybe looking for a yes/no at this time, and if yes, I can probably get a programming person at my company to take a look at it (I guess though that any VBA starting tips would be helpful if yes).

Thanks all for any help!  

Outcomes