AnsweredAssumed Answered

The Thru Method

Question asked by ChengChoyTan on Jun 5, 2007
Latest reply on Jun 5, 2007 by ChengChoyTan
Hello everybody. As we know, the Thru method is defined automatically in the Guided Calibration part in Calibration Wizard each time the DUT type or the Cal Kit is selected in the wizard.

In my case, where the calibration is controlled through programming, i mean the guided calibration using the SCPI commands under SENS:CORR:COLL:GUID, the Thru method is never been defined (stays in DEFAULT) unless i defined it by sending the command SENS:CORR:COLL:GUID:METH.

Is there any way to define the Thru Method automatically through programming? I have try sending the command SENS:CORR:COLL:GUID:METH DEF (which use the THRU definition that is stored in the cal kit file), but it didn't work... Thank you for helping.  

Outcomes