AnsweredAssumed Answered

Need a fast read on 2points on a N5320A

Question asked by ldalep on Feb 25, 2007
Latest reply on Feb 26, 2007 by jvall
Hi .... I read that DCOM is generally faster because there is little parsing of the out going messages from the host like there is with GPIB.  I have an application where I will be looking at a single trigger then 2 points and adjusting the dut based upon this.  I know that it greatly  is dependent on IF and sweep speed  but the best I seem to do is about 16msec/cycle    ->trigger then read.   I am getting blazing speed when there is a large group of data say 32000readings/sec but that comes from large swept 16001 points.  does adding a bridge to the lan help - any suggestions?  

Outcomes